Solution
Friction Testing
A testing laboratory was looking to replace two single axis load cells used in their friction testing machine with one sensor that could measure force on the x, y, and z axis simultaneously.
A testing laboratory was looking to replace two single axis load cells used in their friction testing machine with one sensor that could measure force on the x, y, and z axis simultaneously.
Interface’s 3A60 3-Axis load cell was installed on their existing machine with an Interface BSC4D-USB Multi-Channel PC Interface hooked directly to a PC laptop to monitor and log the data in real time.
The testing laboratory was able to simplify their sensor set-up and improve their data collection, creating more value for their end customer.
Notifications